AXIS#.MT.CNTL

Description

The controlword describes the behavior of the motion task.

Since this parameter is read bitwise, it can combine multiple functions into a single word. The meaning of each bit is described in the tables below.

Table 1: Motion Task (MT) Bit Descriptions

Bit

Meaning

Description

0

0x00001

See Table 2: MT Type. 

1

0x00002

2

0x00004

3

0x00008

4

0x00010

If this bit is 0, then the next MT is not executed.

If this bit is 1, then the next MT is executed.

5

0x00020

See Table 3: Next MT Start Type.

6

0x00040

7

0x00080

8

0x00100

9

0x00200

10

0x00400

See Table 4: MT Acceleration Type.

11

0x00800

12

0x01000

Reserved.

13

0x02000

If this bit is 0, then an attempt to trigger any new motion task will be accepted while this motion task is currently running.

If this bit is 1, then an attempt to trigger any new motion task will be denied while this motion task is currently running.

14

0x04000

If this bit is set, the motion task that is supposed to be started cannot be started from velocity 0. The motion can be started if a motion task already running will be interrupted.

15

0x08000

Reserved.

16 0x10000 The motion task target velocity will be taken from an external source such as an analog input signal.

Table 2:  MT Type

Bits 0, 1, 2, 3

Description

0000

Absolute. The target position is defined by the AXIS#.MT.P value.

1000

Reserved.

0001

Relative to Command Position. The target position is defined as:
Target position = AXIS#.PL.CMD + AXIS#.MT.P

0011

Relative to Previous Target Position. The target position is defined as:
Target position = Target position of the last motion task + AXIS#.MT.P

0101

Relative to External Start Position. The target position is defined as:

Target position = External start position + AXIS#.MT.P

0111

Relative to Feedback Position. The target position is defined as:
Target position = AXIS#.PL.FB + AXIS#.MT.P

Table 3:  Next MT Start Type

Bits 5, 6, 7, 8, 9

Description

00000

Switches over to next MT after stopping. After an MT ends, the next MT starts immediately.

00001

Switches over to next MT after stopping and delay. After an MT ends, the MT following time (AXIS#.MT.TNEXTelapse in order to start the next AXIS#.MT.

00010

Switches over to next MT after stopping and external event. After an MT ends, an external event (such as a high digital input) must occur in order to start the next AXIS#.MT.

00011

Switches over to next MT after stopping, delay, and external event. After an MT ends, the AXIS#.MT.TNEXT must elapse and an external event (such as a high digital input) must occur in order to start the next AXIS#.MT.

00111

Switches over to next MT after stopping, then delay or external event. After an MT ends, the AXIS#.MT.TNEXT must elapse or an external event (such as a high digital input) must occur in order to start the next AXIS#.MT.

10000

Switches over to the next MT while still in motion (change on the fly). After reaching the target position (MT.P), the next MT starts. The drive then accelerates with the adjusted acceleration ramp of this next MT to the target velocity of this next AXIS#.MT.V.

Note: this is not possible if the following motion task is in the opposite direction. If the following task is in the opposite direction, the axis will come to rest before reversing in the opposite direction.


  • This is not possible if the following motion task is in the opposite direction. If the following task is in the opposite direction, the axis will come to rest before reversing in the opposite direction.

11000

Switches over to the next MT while still in motion (change on the fly). After reaching the target position (MT.P), the drive has already accelerated with the acceleration ramp of the next MT to the target velocity AXIS#.MT.V. Thus, the drive begins the next MT at the next MT target velocity.


  • This is not possible if the following motion task is in the opposite direction. If the following task is in the opposite direction, the axis will come to rest before reversing in the opposite direction.

Table 4:  MT Acceleration Type

Bits 10, 11

Description

00

Trapezoidal acceleration and deceleration.

Examples

Code

Modifies the bitfield for motion task 0. The first parameter is the motion task number and the second is the new bitfield to overwrite the existing bitfield

-->AXIS1.MT.CNTL 0 [bitmask]

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write Array

Units

N/A

Range

0 to 4,294,967,295

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MT.CNTL 0

50d7h

01h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 1

50d7h

02h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 2

50d7h

03h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 3

50d7h

04h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 4

50d7h

05h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 5

50d7h

06h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 6

50d7h

07h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 7

50d7h

08h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 8

50d7h

09h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 9

50d7h

0ah

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 10

50d7h

0bh

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 11

50d7h

0ch

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 12

50d7h

0dh

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 13

50d7h

0eh

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 14

50d7h

0fh

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 15

50d7h

10h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 16

50d7h

11h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 17

50d7h

12h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 18

50d7h

13h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 19

50d7h

14h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 20

50d7h

15h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 21

50d7h

16h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 22

50d7h

17h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 23

50d7h

18h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 24

50d7h

19h

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 25

50d7h

1ah

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 26

50d7h

1bh

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 27

50d7h

1ch

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 28

50d7h

1dh

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 29

50d7h

1eh

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 30

50d7h

1fh

Unsigned32

-

-

Read/Write

No

AXIS1.MT.CNTL 31

50d7h

20h

Unsigned32

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6302

1

6302 (0x189e)

AXIS1.MT.CNTL

Unsigned32[32]

Read/Write

Yes

71838

2

6302 (0x189e)

AXIS2.MT.CNTL

Unsigned32[32]

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MT.CNTL

6302

Unsigned32[32]

Read/Write

-